{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

Can a breaker with a Micrologic trip unit be reverse fed (backfed)?

Article available in these languages: Spanish

Issue:
Can a breaker with a Micrologic trip unit or with integral ground fault protection be reverse fed?

Product Line:
Circuit Breakers

Environment:
Powerpact H, Powerpact J, Powerpact L, PowerPact P, Powerpact R, Masterpact NT, Masterpact NW,

Resolution:

1.  All circuit breakers can be reverse fed unless marked LINE and LOAD which restricts them to forward-fed application only.

2.  All Masterpact and Powerpact M, P, and R frame breakers can be reverse fed.  This includes breakers with Micrologic trip units and integral ground fault protection (LSIG trip unit functions).

3.  Powerpact H, J, and L frame circuit breakers with INTERCHANGABLE TRIP UNITS  are marked LINE on the on side and LOAD on the off side, so they can NOT be back fed.

4.  Powerpact H, J, and L circuit breakers with permanent, factory-sealed trip units may be backfed.
  • Exceptions for H and J frames and legacy F and K frames are that if they are used with GFM or ELM modules they are restricted to forward-fed applications only.
5.  Note also that QO and HOM breakers with suffix GFI, EPD, AFI, CAFI, DF, DF and EDB-EPD type breakers can NOT be backfed.

Schneider Electric Australia

Explore more
Category:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: