{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What are the neutral current transformers used for ground fault sensing NT and NW Masterpact breakers?
Product Line:
NT and NW Masterpact breaker

Resolution:

Table 41:        T-Frame Circuit Breakers
External neutral sensor for 3-phase, 4-wire residual ground fault system (or for neutral current monitoring).
These neutral sensors include their wiring harness. To order this harness as a spare part, order cat. no. NCTWIRING.
NT Circuit Breaker
Sensor Plug
External Neutral Sensor for general useExternal Neutral Sensor
Square D Panelboard
External Neutral Sensor for use in
Square D Switchboards
External neutral sensor for circuit breakers with standard neutral protection
100–250 AS33575S33924S33926
400–1600 AS33576S33925S33927
External neutral sensor for circuit breakers with oversized neutral protection♦
100 AS33575S33924S33926
250 AN/AN/AN/A
400–1000 AS33576S33925S33927
1200/1250 AS48896N/ANA
1600 AS48182N/ANA
♦Oversized neutral protection = 1.6xIr where Ir = long time pick-up.


Table 42:        W/Y-Frame Circuit Breakers
External neutral sensor for 3-phase, 4-wire residual ground fault system (or for neutral current monitoring) and external sensor for Modified Differential Ground Fault (MDGF) or Source Ground Return (SGR) system.
These neutral sensors include their wiring harness. To order this harness as a spare part, order cat. no. NCTWIRING.


Frame
Size


Sensor Plug (A)
External Neutral SensorPZ4 External Neutral Sensor
(For use in PZ4 Switchgear)


MDGF/ SGR
Sensor►

For Residual Ground Fault
For 3-Pole Circuit Breaker with
Oversize Neutral
Protection♦

For Residual Ground Fault
For 3-Pole Circuit Breaker with
Oversize Neutral
Protection♦






W
100 S48916S48916 S48902S48902
250N/AN/A
400


S34036

S34036



S48903


S48903




S33579
600/630
800
1000
1200/1250S48896
1600
S48182



N/A
2000S48896
2500

S48182


S48182
3000
N/A
3200
4000N/A




Y
2000



S48897•


S48897•


S48898•

S48898•




S33579
2500
3000


N/A
3200
4000
5000
N/A
S48897•
6000
6300N/A
•Kit includes qty. (2) neutral sensors.
►Four MDGF sensors (phase + 1 neutral) are required for W-frame; eight MDGF sensors are required for Y-frame. For SGR system, only one sensor (neutral) is required for W-frame; two sensors for Y-Frame.
An MDGF/SGR ground fault interface module (Cat. no. S48891) is also required for each circuit breaker.
♦Oversized neutral protection = 1.6xIr where Ir = long time pick-up.

Schneider Electric Australia