Issue:
Obsolete AD module power supply for Micrologic
Product Line:
Circuit Breakers
See instruction bulletin, S1A80373.
As an example, this is a picture of the 685826.
Obsolete AD module power supply for Micrologic
Product Line:
Circuit Breakers
Resolution:
These are now obsolete; information for installed base only
Cat. No. | Input | Output |
685823 | 24–30 Vdc | 24 VDC, 1 A (all have this same output) |
685824 | 48–60 Vdc | |
685825 | 100–125 Vdc | |
685826 | 110–130 Vac | |
685827 | 200–240 Vac | |
685829 | 380–415 Vac |
See instruction bulletin, S1A80373.
As an example, this is a picture of the 685826.