{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Is there a thru the door external operator for the GV2ME and GV2P manual starters?

Issue:
What is the through-the-door operating mechanism for a GV2 Manual starter?

Product Line:
Digest 177 Section 18 : Contactors and Starters - IEC

Environment:
North American Products

Cause:
Needs  the through-the-door operating mechanism for a GV2P Manual starter

Resolution:
There are no available kits for the GV2ME devices, only the GV2P devices (as listed below)
GV2APN01 - Nema 1 Black
GV2APN02 - Nema 1, 12 Red/Yellow
GV2APN04 - Nema 3R, 4, 4X Red/Yellow

Schneider Electric Australia