{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

Can the MotorLogic solid state overload relays be used on single phase applications?

Issue:
Can 9065 Solidstate overload relays be used in single phase applications?

Product Line:
NEMA Contactors and Overload relays

Environment:
9065 solid state relays series F

Cause:
Older MotorLogic solid state overload relays could not be used with single phase applications, but series F units can.

Resolution:
Yes, however only Series F and newer. These units can be used with single phase applications by looping one of the wires so that it passes through all three CTs in the overload.  See page 8 of the attached instruction sheet for an example.

Schneider Electric Australia

Attachment(s)

9065 single phase wiring 30072-013-29_01.pdf9065 single phase wiring 30072-013-29_01.pdf [1.07 MB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: