{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How do you calculate the size of the enclosure required for the ATS48’s to dissipate the heat generated
To calculate the size of the enclosure required for an ATS48 soft start you would use the follow equations

Enclosure thermal calulation
To calculate the figure P use the power dissipated figures from the below tables and add it to the power
dissipated figures of all the other equipment to be housed in the enclosure
For Standard Applications                                For Severe Applications
ATS standard duty selection chart ATS48 severe duty selection chart
You then insert the number calculated for Rth into the calculation below; the Effective exchange
surfaces are those that do not make contact with any other object i.e. floor or wall


heat exchange calculation

It is always advisable to fit a bypass contactor with the ATS48 Soft Starter to
reduce the heat generated


The last two items show the recommended spacing’s around the soft starters and the flow rate of the
fans if fitted into the cabinet.

ATS48 recommended panel mount spacingsATS48 cooling fan flow rates












Schneider Electric Australia