{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

Changing the pressure setting on 9013 pressure switch

Issue:
How can I change the high/low or on/off points on a 9013 pressure switch?

Product Line:
9013 pressure switches

Cause:
It is sometimes necessary to change the pressure settings on the switches from what they have been preset

Resolution:
On all 9013 pressure switches there are one or two adjustment nuts holding a spring inside of the cover.  With the power disconnected to the switch, these nuts can be adjusted to change the pressure switch.  On units with one adjustment nut, this adjustment will change the high and low setting at the same time.  On units with two adjustment nuts, the larger spring controls the high and low setting.  The smaller spring controls the differential (spread) between the high and low points.  Reference the attached troubleshooting guide for specific adjustment instructions.

Schneider Electric Australia

Attachment(s)

9013DB0701 - 9013 Troubleshooting.pdf9013DB0701 - 9013 Troubleshooting.pdf [99.56 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: