{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What are the part numbers for the adjustable rating plugs for the Compact NS630B- NS3200, Powerpact P and R frame breaker, and the Masterpact NT and NW breakers?
Inquiry:
Rating plugs for Micrologic breakers

Product Line:
Molded Case Circuit Breaker

Resolution:
Interchangeable rating plug catalog numbers are as follows:

Long-Time Pick-Up Ir = In  x  ... (dial setting below)
Table showing rating plug part numbers

Schneider Electric Australia