{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

What is the operation of the GVAD fault signalling contacts of the GV2 & GV3 motor protection circuit breakers?

GV2 & GV3 motor protection circuit breakers (MPCB) can be fitted with the following fault indicating contact blocks:

GVAD0110
GVAD0101
GVAD1010
GVAD1001

These blocks comprise fault signalling contacts and instantaneous auxiliary contacts.

GVAD0110
A N/C fault signalling contact (terminals 95-96), closed if there is no fault, open when a fault (magnetic or thermal) occurs.

A N/O instantaneous auxiliary contact (terminals 53-54), closed when the device is energised and open when the device is de-energised.

GVAD0101
A N/C fault signalling contact (terminals 95-96), closed if there is no fault, open when a fault (magnetic or thermal) occurs.

A N/C instantaneous auxiliary contact (terminals 51-52), closed when the device is de-energised and open when the device is energised.

GVAD1010
A N/O fault signalling contact (terminals 97-98), open if there is no fault, closed when a fault (magnetic or thermal) occurs.

A N/O instantaneous auxiliary contact (terminals 53-54), closed when the device is energised and open when the device is de-energised.

GVAD1001
A N/O fault signalling contact (terminals 97-98), open if there is no fault, closed when a fault (magnetic or thermal) occurs.

A N/C instantaneous auxiliary contact (terminals 51-52), closed when the device is de-energised and open when the device is energised.

How to test:
The instantaneous auxiliary contact test is performed by creating a state of transition of the handle actuator between the de-energised position and the energised position.

The fault contact test is performed by pressing the test button when the handle actuator is in the closed position.

Schneider Electric Australia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: