{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Replacement contacts for XALK control stations
Issue:
Which contacts are used with the XALK control stations

Product Line:
XALK control stations

Environment:
Maintenance

Cause:
There are multiple ways of adding contacts to these stations

Resolution:
The control stations use ZENL1111 (NO) and ZENL1121 (NC) contacts standard.  Regular 22mm contacts (ZBE series) can also be used with these control stations provided that a mounting collar is also used.

Schneider Electric Australia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.