{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What are the red safety covers for the TeSys D LC1D contactors?
Issue:
What is the red safety cover for D line contactor.

Product Line:
D-Line IEC contactors

Environment:
IEC Contactors sold and used in the United States

Cause:
Requirement for safety covers in specific situations

Resolution:
LAD9ET1S for 9A to 65A contactors.
LAD9ET3S for 80A to 95A contactors.
LAD9ET4S for 110A to 150A contactors.
There are also auxiliary contacts available for front mount with a ref cover, model LADN22S, 2NO + 2NC

Schneider Electric Australia