{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
New design for XB4/XB5 mushroom buttons
Issue:
The appearance of the XB4/XB5 and ZB4/ZB5 pushbuttons have changed, What is the difference?

Product Line:
Push Buttons and Operator Interface

Environment:
22mm Harmony Pushbuttons

Cause:
Design change

Resolution:
All of the 22mm mushroom head maintained pushbuttons have changed as part of a refresh of the line.  The newer units which have a yellow bezel are the newer units.  Besides these cosmetic changes, there are no form, fit, or functional differences.

Schneider Electric Australia