Do Clipsal have a 20a single module RCBE @ 10ma suited for hospital use ?
Yes we do , In this case it would be the 4RCBE220/10S. To be approved for use in hospitals the RCBO must be approved as "Type 1" (ie: 10mA sensitivity, switch both Neutral and Active, and trip in <40ms) The below range of Slimline RCBO's are rated as Type 1 and therefore compatible
For more information on Clipsal Circuit protection please visit the Clipsal web site on the provided link http://www.clipsal.com/Trade/search-results?q=circuit%20protection
Released for:Schneider Electric Australia
Explore more
Range:
Acti9 iC60 RCBO
Explore more
Range:
Acti9 iC60 RCBO
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.