{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

How to change the power sign on 5.2E, 6.2E, 5.3E,6.3E trip units for Powerpact H, J and L frame breaker?

Issue:
How to change the power sign on 5.2E, 6.2E, 5.3E,6.3E trip units for Powerpact H, J and L frame breaker?

Product Line:
Powerpact H, J and L

Resolution:
The power sign can be changed through Modbus registers or with RSU software and UTA test kit STRV00910.

RSU:
Modify the Power sign using the RSU software and UTA Tester STRV00910, see link for free RSU download.
https://www.se.com/us/en/download/document/Micrologic_RSU_Compact+NSX_rev_13.3.2_Setup/

In the Metering setup/Power sign window, select the power sign:
• + The power running through the circuit breaker from top to bottom is
counted positively.
• - The power running through the circuit breaker from top to bottom is
counted negatively.
The default value of the power sign is +.


MODBUS:
Power Flow
Sign 3316 3315 RW — — UINT 0–1 E
Power flow sign
0 = the active power flows from upstream (top) to downstream (bottom) (default).
1 = the active power flows from downstream (bottom) to upstream (top).
The power flow sign command (command code = 47240) configures the content of the power flow sign register.

8000 7999 — — UINT 46240 E Command code = 46240
8001 8000 — — UINT 12 E Number of parameters (bytes) = 12
8002 8001 — — UINT 5121 E Destination = 5121 (0x1401)
8003 8002 — — UINT 1 E 1
8004
8005
8003
8004 — — STRING — E Level 4 password (default value = ‘0000’ = 0x30303030)
8006 8005 — — UINT 0–1 E
Power flow sign
0 = the active power flows from upstream (top) to downstream (bottom)
(default)
1 = the active power flows from downstream (bottom) to upstream (top).

Schneider Electric Australia

Attachment(s)

Power Setup from Micrologic 5 and 6 trip unit user guide 48940-312-01 1-2012.pdfPower Setup from Micrologic 5 and 6 trip unit user guide 48940-312-01 1-2012.pdf [86.5 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: