{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Difference Between the XENG1191 and the XENG1491
Issue:
What is the difference between the XENG1191 and the XENG1491?

Product Line:
22mm Pushbuttons - GIC Product

Environment:
US Product

Cause:
Specific identification of contact blocks

Resolution:
The XENG1191 is a two speed contact block with 1 NO early close as well as 1 standard NC and 1 standard NO.  The XENG1491 is a single speed contact block with 2 NO and 1 NC standard contacts.

Schneider Electric Australia

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: