{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Is the undervoltage release (UVR or MN) for the Powerpact M, P, and R frame breakers kiss free?
Issue:
If the UVR is not energized, will the main contacts touch when an attempt is made to close the breaker?

Product Line:
Circuit Breakers

Resolution:
They are kiss free. If the undervoltage trip is not energized, it is impossible to close the circuit breaker either manually or electrically. An attempt to close the circuit breaker produces no movement of the main contacts.

Schneider Electric Australia

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: