{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
​What is the difference between the IFE (LV434001) and IFE Gateway (LV434002)?
Issue:
Distinguish between IFE switchboard server and IFE ethernet interface

Product Line:
Smart Systems

Resolution:
The IFE and the IFE Gateway appear very similar (see picture below), but there is a difference.
  • The IFE (cat. no. LV434001) is the Ethernet interface for Powerpact and Masterpact circuit breakers.  Previous cat. no. was LV434010.
  • The IFE Gateway (cat. no. LV434002) is the Ethernet interface for Powerpact and Masterpact LV circuit breakers, plus a gateway for Modbus-SL (serial line) connected devices. Note that the IFE Gateway is also referred to as IFE Modbus, or IFE Server. Previous cat. no. was LV434011.


IFE and IFE-Gateway

Schneider Electric Australia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: