{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What do 16A & 6AX ratings mean on the PDL600RM?
It means the relay module can switch a load of up to 16A resistive or a 6A fluorescent or Inductive  load.

https://www.se.com/nz/en/product/PDL600RM/relay-module-600-series---240-v---6-ax/

Schneider Electric Australia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: