{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Can you use a two pole GFI as a single pole?
Issue:
QO 2p as 1p breaker

Product Line:
Circuit breakers

Resolution:
Yes, you can. We recommend using the pole that contains the push to test button, otherwise the test function won't work.

Schneider Electric Australia