undefined undefined
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

Are Acti9 iC60 MCBs suitable for DC applications?

Yes, Acti9 iC60N/H MCBs are suitable for DC applications ranging from 12VDC to 250VDC subject to the number of poles connected in series and the required breaking capacity.
The attached document shows the number of poles that are required to be connected in series in relation to the supply voltage and the breaking capacity that is achieved.

Schneider Electric Australia

Attachment(s)

Acti9_iC60.pdfActi9_iC60.pdf [184.02 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: