{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What can cause an E21 fault on the Altivar ATV21 and ATV212 drives?
Issue:
E21 fault code on ATV21 and ATV212

Product Line:
Altivar ATV21 and ATV212

Environment:
All

Cause:
Drive powers up with an E21 CPU is failing

Resolution:
The E21 is a CPU error 2 fault.   If you power cycle and the fault does not clear the drive will need to be replaced.

Schneider Electric Australia