How can we help you today?
Can the LED on the 30PBL switch operate without a neutral at the switch?
Yes the 30PBL can have LED indication without a neutral present. Due to having no neutral present, you can only achieve LED indicator "ON" when load is "OFF".
![30PBL 30PBL](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000007ulqbQAA&oid=00DA0000000abSm)
Some of the key features are:
Some of the key features are:
- Blue LED indicator
- One way/two way switching facility with loop terminal
- Retrofit option in to any 30 series aperture
- Suitable for fluorescent loads Up to 16AX
- Shrouded in-line Terminals provide protection during installation
Released for:Schneider Electric Australia
Explore more
Range:
Explore more
Range: