{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Reset Button: combination starter with Tesys T
Issue:
If a combination starter is ordered with a Tesys T overload relay will the door of the enclosure have a reset button?

Product Line:
Combination Starters

Environment:
NEMA Combination Starters

Cause:
Product Characteristics


Resolution:
Yes it will, unless the combination starter comes in a NEMA 12/3R which specifically excludes a reset button on the door. This can be seen by looking at the combination starter class and type in the Schneider Electric Digest.

Schneider Electric Australia