{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

Do we offer a make before break contacts on the 9001 pushbuttons

Issue:
Do we offer a make before break contacts on the 9001 pushbuttons

Product Line:
9001

Environment:
Pushbuttons

Resolution:
9001KA4 contact block is has a NO Early Closing contact and a standard NC which will make before the NC contact breaks in one contact. The 9001KA6 is an early closing NO contact only. When installed in tandem to a 9001KA3 (or a 9001KA1) the 9001KA6 will close before the opening of the NC contact.

Schneider Electric Australia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: