{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Does the Cloud Connected EVlink Charging Station have a wired connection?
Issue:
Customer is looking to connect via a LAN connection.

Product Line:
EVlink Charging Stations

Resolution:
Cloud connected stations only connect to the cloud(internet) via a cellular modem.  No hardwired connection (ethernet) is available.
In many situations the areas where EV stations are installed do not have access to LAN (local area network) connections.  This
also allows the stations to be installed without any issues concerning security of the LAN.
Cloud Connected Station

Schneider Electric Australia