{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

How many IFMs can be stacked to an IFE switchboard server (LV434002)?

Issue:
What is the maximum number of IFMs that can be attached to the IFE switchboard server using the stacking modules?

Product Line:
Smart Systems

Resolution:
Up to 12 IFMs can be stacked to an IFE switchboard server (LV434011 or LV434002) via the stacking module.

Schneider Electric Australia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: