{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

Are QO and HOM DF dual function breakers available in 2 poles?

Issue:
Needing 2pole Dual function breaker for 240V loads.

Product Line:
Miniature Circuit Breakers

Resolution:
No, QO and HOM DF dual function breakers are not available in a 2 pole version. They are available in single pole only.
What is available are 2 pole versions of GFI ground fault breakers.

Schneider Electric Australia