{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Video: How does the PK4MB2HA retaining kit install into the proper QO, single phase, 225 A max, convertible mains load centers?
Issue:
Product Design Features 
 
Product Line:
QO Load Centers
 
Resolution:
The PK4MB2HA retaining kit secures one QO 2-pole branch circuit breaker with or without electrical accessories to the Right side of the interior when used as a Back-Fed Main Breaker.
This retaining kit can ONLY be used for QO, 1phase, 150-225amp, Convertible main load centers, Series S01 and S02, and Plug-On Neutral Series S06 Load Centers.
The retaining bracket will mount over the face of the back-fed branch breaker and get secured using the single interior mounting screw that comes with the kit.
NOTE: QO-GFI and QO-AFI branch circuit breakers are NOT suitable for use as back-fed main circuit breakers.

The attached video is ONLY to supplement the INSTRUCTIONS that come with the kit. Please make sure to read the instructions and all the below Safety Information that is located in the instructions BEFORE working on any electrical equipment.
A pdf copy of the complete instructions is attached below the video.
Danger label pic

Make sure to turn OFF ALL Power supplying the equipment and verify the power is OFF using a properly rated voltage sensing device, BEFORE working on or with electrical equipment. 
1) Once all Safety steps are followed, begin the kit installation by following the instructions.
2) Make sure to obtain the correct 2-pole, QO branch breaker to be used as the back-fed Main and DO NOT exceed the maximum rating marked on each load center.
3) As shown in step 2, on page 2 of the instructions, remove and discard the interior mounting screw(Fig. 1) 
4) Install the appropriate  QO back-fed branch breaker ONLY in positions 2-4 (The first two positions in the upper right side of the interior)
5) Center the retaining bracket over the breaker to be used as the back-fed breaker and press down against the face of the retaining bracket to seal it against the breaker.
6) Secure the retaining bracket to the base with the new interior mounting screw provided in the kit and torque to 35 lb-in (4 N-m)
7) Remove the backing of the wiring diagram label that comes in the kit, to expose the adhesive and attach the label to the inside of the load center enclosure or to the back of the cover.

NOTE: PLEASE READ ALL INSTRUCTIONS AND SAFETY INFORMATION THAT COME WITH THE KIT AND NEVER WORK ON ENERGIZED EQUIPMENT.

Schneider Electric Australia

Attachment(s)
PK4MB2HA instructions.pdf [161.17 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
move-arrow-top
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.