{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What length sizes are available for the Momentum interbus I/O bus cables?
Issue
Momentum interbus cable lengths

Product Line
Modicon Momentum

Resolution
The Momentum interbus I/O bus cable is only available in two lengths.....

170MCI00700 - Interbus (I/O Bus) cable 11cm long (4.3")
170MCI10001 - Interbus (I/O Bus) cable 100cm long (40")

Schneider Electric Australia