{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the RAL number and part number for the cream paint used on the Powerpact 4 panelboards?
The cream colour paint used on the Powerpact 4 panelboards is RAL9001.

We used to offer an aerosol can Part Number 08962 or Touch up paint part Number 08961, but they have ended.

Schneider Electric Australia

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: