{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What does B,C,D curve mean for Acti 9 MCB?
B Curve means the MCB trips between 3-5 times full load current. It is mainly used in residential applications where loads are resistive e.g. lighting fixtures, domestic appliances with low surge Levels.
C Curve means the MCB trips between 5-10 times full load current. It is used  in commercial/industrial applications where there is greater chances of higher short circuit currents e.g. mainly inductive loads , fluorescent lighting.
D Curve means the MCB trips between 10-14 times full load current. It is used where inrush currents can be very high e.g. motors, X-ray machines.
Here is the curves diagram:
Curve Diagram

Schneider Electric Australia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: