{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Is there a product available to stop LED flickering?
If you are experiencing flickering LED loads when dimming to low levels the 31LCDA has the potential to reduce and/ or remove the flickering. It is important to note that this device isn't guaranteed to remove flickering, it is designed to help with compatibility. If you don't achieve removal of flickering it is possible to stack a total of 3, 31LCDA's in parallel. If you are still experiencing issues once you have placed 3 in parallel your LED loads may just be incompatible and replacement of the LED loads may be necessary.

Some of the key features are:
  • 450W maximum load.
  • Potential removal of flickering.
  • Indoor use only.
  • Operating temperature 0°-65°C.
  • 220-240V A.C. typical, 50Hz only.
  • Dimensions 30mm (W) X 20mm (H) X 10mm (D).
  • Flylead length approx. 95mm
For further information please visit http://www.clipsal.com/Trade/Products/ProductDetail?catno=31LCDA
LED

Schneider Electric Australia