{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the difference between the iC60N and the iC60H Circuit Breakers?
The differences between the iC60N and iC60H series of circuit breakers is the iC60N has a breaking capacity of 6kA at 240/415V, C Curve in accordance with AS/NZS60898.1, where as the iC60H has a breaking capacity of 10kA at 240/415V B, C & D Curve in accordance with AS/NZS60898.1.

In Australia the iC60N is only available in C Curve where as the iC60H is available in B, C & D Curve.

iC60N & iC60H Dimensions

Connection: Tunnel terminals for the following cables
- up to 25A : 25mm2 stranded
- 32 to 63A : 35mm2 stranded

For further information please visit https://www.se.com/au/en/product-subcategory/1605-acti-9-miniature-circuit-breakers---mcbs/


Schneider Electric Australia