How can we help you today?
ETSNZ Can the EVlink Wallbox be controlled over ethernet using Modbus CTP/IP or Ethernet TCP/IP on a residential Installation?
You can control it using OCPP with either Modbus TCP or Ethernet TCP.
The appropriate port in the sites router will need to be opened to be able to gain access over the controller.
You can control the current limitation on the device
The appropriate port in the sites router will need to be opened to be able to gain access over the controller.
You can control the current limitation on the device
Released for:Schneider Electric Australia
Explore more
Range:
Explore more
Range: