{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

Can you wire multiple 750WPR 3-wire sensors in parallel?

Yes, you can wire multiple 3-wire 750WPR sensors in parallel as they are a 3-wire device and aren't load dependant.
Some of the key features are:

  • 10A maximum load current
  • Stand-by power consumption is less than 1W
  • 3 Wire
  • Neutral required
  • 30 seconds warmup time
  • 18 metre radius x 110° rated detection field at maximum sensitivity
  • 5 seconds to 20 minutes timer delay range
  • Cables accommodates 4 terminals, up to 2 x 2.5mm² cable per terminal
  • Relay switching method

For further information please visit www.clipsal.com/Trade/Products/ProductDetail?catno=750WPR

Schneider Electric Australia

Explore more
Range:
Lighting Accessories
Explore more
Range:
Lighting Accessories
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.