Issue: Time delay feature for digital inputs in the ATV630/930 Product line: Altivar Process ATV630 ATV930 Environment: All models Cause: n/a Resolution: All of the digital inputs have an ON Delay setting range of 0-200msec. The factory default is 0msec. Under Complete settings -> Input/Output -> DI/DQ -> DIx Config, set DIx Delay to the desired time delay. This delay setting works only as an ON delay, for DIx going active. There is not a delay feature for OFF delay. |
Released for:Schneider Electric Australia