How can we help you today?
Do the PM5500 series meters support BACNet MSTP protocol?
Issue
Do the PM5500 series meters support BACNet MSTP protocol?
Product Line
PM55xx
Resolution
The PM5500 series meters do not support BACNet MS/TP (BACNet Serial), these meters only support BACNet IP (over Ethernet)
Kindly refer to page 54 the PM5500 User Manual for more details on BACNet IP support.
Do the PM5500 series meters support BACNet MSTP protocol?
Product Line
PM55xx
Resolution
The PM5500 series meters do not support BACNet MS/TP (BACNet Serial), these meters only support BACNet IP (over Ethernet)
Kindly refer to page 54 the PM5500 User Manual for more details on BACNet IP support.
Released for:Schneider Electric Australia
Explore more
Range:
Explore more
Range: