undefined undefined
{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What are the System requirements for Unity Pro V13?
System with Microsoft Windows 7 Professional 32/64bits
System: Pentium Processor 2.4 GHz or higher, recommended 3.0 GHz
RAM memory: 2GB minimum; recommended: 4GB
Hard disk: minimum available free space 8 GB, recommended 20 GB
Microsoft Internet Explorer 5.5 or higher
On Windows 7 64bits System, installation of Windows 7 Service Pack 1 (SP1) is mandatory in order to use Unity Pro V13
 
Windows 7  64bits is recommended for projects using DTMs (example : projects using Modicon M580 controller)
 
 
System with Microsoft Windows 10 32/64bits
System: Pentium Processor 2.4 GHz or higher, recommended 3.0 GHz
RAM memory: 2GB minimum; recommended: 4GB
Hard disk: minimum available free space 8 GB, recommended 20 GB
Windows 10  64bits is recommended for projects using DTMs (example : projects using Modicon M580 controller)
 
System with Microsoft Windows Server 2012 R2
Recommended version: Windows Server 2012 R2, standard version
Processor recommended: 3.20GHz
RAM memory recommended: 16.0 GB
 
Important notice
Unity Pro requires .NET 3.5 and .NET 4.5.2
Depending on the target Windows version and Windows configuration, .Net versions may be
      - not installed
      - installed but not enabled ( the related "windows feature"  is not set ON )
      - installed and enabled
 
Unity Pro setup tries to automatically install and enable the required .Net  on the target Windows if necessary.
 
On Windows 10 and Windows Server 2012 R2, automatic or manual installation of .Net 3.5 requires an internet connection.
And service “Windows Update” must be started in order to install the .NET Framework 3.5.
 
If automatic installation of  .Net 3.5  fails, please read & follow  Microsoft technical notes on .NET 3.5 installation:
 
      - Installing the .NET Framework 3.5 on Windows 8 or 8.1
      http://msdn.microsoft.com/en-us/library/hh506443.aspx
 
           
 
Virtualization:
Unity Pro V13 has been successfully tested in the following configuration :
  • VirtualBox 5.0.20
  • VMware Workstation 12 Pro 12.1.0 build-3272444
 
 
DVD-ROM drive: to install the software;
DVD-ROM writer recommended
 
Display:
Min VGA (800-600).
Recommended:
·         SVGA (1024-768 or more) with high color 24 bits
·         SVGA (1280-1024 or more) for Windows 10 and Windows Server 2012 R2
 
Pointing device:
Mouse or compatible devices. 
Access rights on the computer
Unity Pro V13 needs to have Administrator access right for installing the software.
For Unity Pro usage User access right are sufficient
Nevertheless Administrator rights must be used for updating the Hardware catalog (CANopen, DTM)
PRM DTM requires administrator rights to work correctly.
 
Note: 
-       User must check that all directories used by Unity pro are accessible in read write mode.
                           Check for the Options Management: Options / General / Paths:
- Project Path
- Import / Export file path
- XVM path
- Project settings templates path
- Project settings template file
- Custom Library path
- Working drive
- Log file path
Check the directory c:\UnityProTemp (Hidden directory) has the following rights: Read, Execute and Write.
 
If these paths are not accessible an error message will appear and the requested operation will fail


-       Access rights & Multi instances : As some components are shared, when several instances of Unity Pro are launched, rights access must be the same on all the instances
-       In Windows 7 , if UAC (User Account Control) is set, and if Unity Pro is executed without checking "Run as Administrator", system folders can be only be accessed in read only and FFB Libset can not be modified.
-       Start Menu: following short cuts must be executed with “Run as Administrator”:
- Remove Unity Pro
- Repair Unity Pro
- Types Library Update


Unity Pro V13 Readme file is attached.




 

Schneider Electric Australia

Attachment(s)
Readme.html [389.38 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
move-arrow-top