Issue:
How many ON-OFF operations can a circuit breaker withstand?
Product Line:
Square D, Powerpact, Masterpact
Resolution:
This table lists the UL endurance test requirements for different frame sizes:
How many ON-OFF operations can a circuit breaker withstand?
Product Line:
Square D, Powerpact, Masterpact
Resolution:
This table lists the UL endurance test requirements for different frame sizes:
Frame Size (A) | Full Load Operations | No Load Operations |
0-100 | 6,000 | 4,000 |
101-225 | 4,000 | 4,000 |
226-600 | 1,000 | 5,000 |
601-800 | 500 | 3,000 |
801-2500 | 500 | 2,000 |
2501-4000 | 400 | 1,100 |
Released for:Schneider Electric Australia