{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

Does a circuit breaker close if the UVR (MN) is not energized?

Issue:
Does a circuit breaker close if the UVR (MN) is not energized?

Product Line:
Masterpact, Powerpact, Legacy Circuit Breakers

Resolution:
No. This release instantaneously opens the circuit breaker when the supply voltage drops below a value between 35% and 70% of rated voltage. If the release is not energized, the circuit breaker cannot be closed (either manually or electrically). Any attempt to close it will have no effect on the main contacts. Closing is possible when the release voltage reaches 85% of its rated value.

Schneider Electric Australia

Explore more
Category:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: