{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

Are the Masterpact NW and NT shunt trip and shunt close coils continuous duty rated?

Issue:
Does the Masterpact NW shunt trip and shunt close have a coil clearing switch?

Product Line:
Masterpact NT and NW breakers

Resolution:
Yes, the coils themselves are continuous duty rated and do not use a coil clearing switch. However, in actual use, a maintained signal should not be used on the shunt close coil (XF). Any opening order will open the breaker so a standing close order is not necessary. Instead, use a signal of at least 200 ms on the shunt close coil (XF) then remove the signal.

Schneider Electric Australia