{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

What is the operating voltage tolerance, catalog numbers, and clearing times for the Masterpact NT and NW shunt trip and shunt close coils?

Issue:
What is the operating voltage tolerance, catalog numbers, and clearing times for the Masterpact NT and NW shunt trip and shunt close coils?

Product Line:
Masterpact NT NW

Resolution:
Shunt trip: operating threshold is 0.7x to 1.1x Vn (nominal voltage)
Shunt close: operating threshold is 0.85x to 1.1x Vn
Catalog numbers are the same for MX and MN (shunt trip and shunt close) devices; function is determined by placement in the breaker.
Voltage (V) at 50/60 HzT-, W-, & Y-Frame FixedT-Frame DrawoutW- & Y-Frame Drawout
12 DCS47359S33809S48490
24-30 AC/DCS47360S33810S48491
48-60 AC/DCS47361S33811S48492
100-130 AC/DCS47362S33812S48493
200-240 AC/DCS47363S33813S48494
277 ACS47364S33814S48495
380-480 ACS47365S33815S48496

MX operating time at Vn:  50 ms ±10 (NW and NT)
XF operating time at Vn:
70 ms ±10 (NW ≤ 4000 A)
80 ms ±10 (NW > 4000 A)
55 ms (NT)

NOTE: Shunt trip (MX) and shunt close (XF) circuits must be energized for a minimum of 200 ms. In other words, don't use an impulse signal. Use a signal of at least 200 ms.

Schneider Electric Australia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: