{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

What is the front mounting kit for a C60N breaker?

Issue:
Is there a front mounting bracket for Multi 9 DIN rail mounted circuit breakers?

Product Line:
Circuit Breakers

Resolution:
Front mounting brackets are available for Multi 9 C60 breakers. There are separate ones for 1P, 2P, 3P, and 4P breakers. Only one breaker can be mounted in one front mounting bracket. Each kit comes with 2 screws to mount the bracket and the proper number of terminal screw shields. The brackets are made of zinc plated steel. The thickness is 1.5 mm. Here are the part numbers:
1P - MG26983
2P - MG26984
3P - MG26985
4P - MG26989

Schneider Electric Australia