{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Are the XB4 and XB5 rated for outdoor use ?
Issue:
Can we use the XB4 and XB5 outside?

Product Line:
XB4 and XB5 push buttons, 22MM

Environment:
Enclosed 22MM push buttons

Resolution:
Yes, when used in a suitable enclosure. They have a NEMA rating of 4 X.

Schneider Electric Australia