{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

Multi-9 C60 Breakers: Values for watts loss and voltage drop per pole

Issue:
Power Loss

Product Line:
Circuit Breakers

Resolution:
The attached document gives the power loss (watts loss) and voltage drop per pole at rated current of the breaker (nominal current). For example, a 1 A breaker would be expected to have a watts loss per pole of 2.3 W at rated current of 1 A. This information can be used to calculate voltage drop when used at other than nominal current.

Schneider Electric Australia

Attachment(s)

C60 watts and voltage loss per pole - UL489 and UL1077 devices.pdfC60 watts and voltage loss per pole - UL489 and UL1077 devices.pdf [65.3 KB]