{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

Do the Micrologic 6.0A, 6.0P, and 6.0H trip units have a ground fault test button? If so, where is it?

Issue:
Does the MICROLOGIC 6.0A / 6.0P / 6.0H trip unit have a ground fault test button and where is it?

Product Line:
Circuit Breakers

Resolution:
The Micrologic 6.0A, 6.0P and 6.0H trip units have a ground fault test button on the front of the trip unit that can be used to satisfy NEC230-95(c). The button is white with a ``T`` in the center of it, and is located between the Ii Instantaneous adjustment dial and the port for the secondary injection test kit cable. See the picture below showing the test button and the instructions below for the testing procedure to meet NEC230-95 (c). The latest requirements may require primary injection testing to verify the operation of the ground fault circuit. Your local inspector will indicate if this is required.

Equipment Ground-Fault Trip Functions Testing
Paragraph 230-95 (c) of the National Electrical Code requires that all equipment ground fault protection systems be tested when first installed. With the circuit breaker closed, test the ground fault trip functions. For instructions on how to close circuit breaker, refer to the circuit breaker installation instructions shipped with the circuit breaker. As of the 2017 NEC230-95(c), the ground fault system needs to primary injection tested. The Test button as described below is no longer accepted for the initial acceptance testing. However, if subsequent testing is desired, the Test button can be used.

Testing ground fault trip with the T test button
1. Make sure the trip unit is powered (it is powered when the trip unit screen shows a display). This can be done by either of the following methods:
  • Apply 24 Vdc to terminals F1 and F2 on the green terminal strip on top of the trip unit (F2 positive). The trip unit will be powered all the time.
  • Connect the trip unit to the Full Funciton Test Kit or Hand Held Test Kit. When the test kit is turned on, the trip unit is powered.
2. Press the T ground fault test button. Circuit breaker should trip.
3. If circuit breaker does not trip, contact the local field office.

Trip unit picture showing test button

Schneider Electric Australia