undefined undefined
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

Can the GV2 be used on single phase applications?

Issue:
Can the  GV2 be used on single phase applications?

Product Line:
Tesys Contactors and Overload Relays

Environment:
All Products

Cause:
Application Assistance

Resolution:
Yes, however you must verify that the device in question is suitable for the load to be controlled. Additionally, because these devices have single-phase sensitivity, provisions must be made to ensure nuisance tripping does not occur due to single phasing. This can be accomplished by wiring the current in series whereas all three poles of the device pass the current.

Schneider Electric Australia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: