{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

Do we have a flush plate like the 9001K25 for 22mm operators?

Issue:
Identifying a 22 mm flush plate

Product Line:
22mm Harmony Pushbuttons

Environment:
Pushbuttons and Operator Interface

Resolution:
We have the XAPE flush plates for the 22mm, but they will not mount to standard wall gang boxes like the 9001K25.

Schneider Electric Australia

Attachment(s)

Flush plates 22mm.pdfFlush plates 22mm.pdf [151.63 KB]
Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: