{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

Can the single pole LA1DN and LADN auxiliary contact module be mounted on the TeSys contactors?

ISSUE
In which contactors can the LA1DN and LADN auxiliary contacts be mounted?

PRODUCT LINE
Auxiliary contacts for the Tesys D line

ENVIRONMENT
Tesys D-Line and Tesys F

RESOLUTION
These contacts will only fit on the following contactors:
Front mount only for LC1D40 through LC1D115 devices and LC1D40A - LC1D65A.
Left side mount only to LC1F contactors

Schneider Electric Australia