{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What are the main differences between Micrologic X and Micrologic 2/5/6/7 ?
Micrologic X control unit is designed and dedicated for MTZ range only. It is an advanced control unit and comes embedded with features such as Bluetooth, NFC and a USB-C port whereas Micrologic 2/5/6/7 didn’t have these features.
Micrologic 2/5/6/7Micrologic X
A, E, P, HX

Micrologic X is customizable through Digital Modules (can be purchased through GoDigital ).
It has EcoStruxure Power Device App smartphone app feature for easy operation and maintenance.
https://www.se.com/au/en/work/products/product-launch/ecostruxure-power-device/
It has a USB-C port and it uses EPC - EcoStruxure Power Commission software for testing, commissioning and reporting.
https://www.se.com/au/en/work/products/product-launch/ecostruxure-power-commission/#Features%20and%20Benefits

Micrologic3.gif

Schneider Electric Australia